Axis Overview
Selecting an Axis in the navigation tree display the Axis Overview screen.
You can view or edit the following information from the Overview window.
|
Button or Dialog Box |
Description |
Parameter |
Parameter |
|---|---|---|---|
| Index | Displays which axis (1 or 2) is selected. | ||
|
Name |
Names each axis in use with a unique identifier. |
||
|
Axis State |
The axis is active when it is enabled and also supplies voltage to the motor. |
DRV.ACTIVE | |
|
Enable |
Click Enable to turn on the power stage in the drive and apply voltage to the motor. |
DRV.ENDEFAULT | |
|
Disable |
Click Disable to turn off the power stage and remove the voltage applied to the motor. |
DRV.ENDEFAULT |